How to set clock to 48Mhz (KL25Z4)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set clock to 48Mhz (KL25Z4)

963 Views
frederik_sebast
Contributor II

Board: KL25Z4

 

Hey, 

 

me and my team are having problems setting the clock from the default mode to 48 Mhz using the external crystal that the the board comes with.

 

I saw that there is a clock set up routine in the start up code (system_MKL25Z4.c and system_MKL25Z4.h) already given and that a routine will be executed based on the definition of CLOCK_SETUP which is not defined by default. So I just defined CLOCK_SETUP as 2 in order to go into PEE mode and have a clock frequency of 48 Mhz. However, when I run the code, reset mode is entered. 

 

So how can I make the system set up to run with 48 Mhz clock frequency?

 

Any help here is appreciated! Thank you very much.

 

Best regards,

Frederik

0 Kudos
0 Replies