AnsweredAssumed Answered

Can't build AVS for Jethro or Morty on IMX7d

Question asked by Martin Leisner on Mar 3, 2019
Latest reply on Apr 13, 2019 by Martin Leisner

Following the instructions here:

Build Alexa SDK (AVS) image for i.mx7D PicoPi board (using Jethro Yocto) 

when I try to build for Jethro, I have a problem fetching the kernel (the tag is unknown)

The original kernel rev was:

d2e98efca60e21ad1b835f0960b5d86009356d69

that's not there anymore (it worked about a month ago),

I had to use:

cca1dee462d96ccabcf072a1d2d4a00ba50f2d81

which looked like an equivalent commit (close to the same comment, but not exactly) -- I still need to compare the kernels manually.

I'm just puzzled how a commit went away (same git repo, same branch).

 

When I build morty with these instructions:

Build Alexa SDK (AVS) image for i.mx7D PicoPi board (with Yocto Morty, Kernel4.9) 

I can't enable AVS.

When I execute the rule:

ERROR: avs-image-1.0-r0 do_rootfs: Function failed: do_rootfs

I get:

1704:Installing perl-module-e.. ######################################## [ 99%]
1705:Installing perl-module-e.. ######################################## [ 99%]
1706:Installing perl-module-e.. ######################################## [100%]
error: Unknown error

util-linux-sfdisk
util-linux-sulogin
util-linux-swaponoff
util-linux-umount
v4l-utils

 

Naturally, unknown error isn't very helpful.

Outcomes