Further details of the SCP command of the SPT 2.0 core

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Further details of the SCP command of the SPT 2.0 core

1,220 Views
andreas_schibil
Contributor I

I'm trying to get as much information from the Reference manual of the S32R274, but the following points are still unclear:

  1. Does the scalar product SCP command (8 coefficientc case ) "dst_addr" support unaligned addresses (not a multiple of 8), e.g. 0x8001?
  2. Will the SCP command (8 coefficient case) and vec_len > 8 store the resulting values at consecutive addresses? Unaligned or at multiples of 8?
  3. Does "dst_addr_inc" support unaligned addresses (not a multiple of 8)? E.g. "dst_addr=0x8000 and dst_addr_inc=2" will store results at 0x8000, 0x8002, 0x8004,... or at 0x8000, 0x8010, 0x8020,... ?

Many thanks for any help!

Tags (4)
0 Kudos
0 Replies