Actually, I have a hikey lemaker board.
So i want to connect hikey board with PN7150. But hikey board just supports 1.8v supply( doesn't support 3.3v ).
When i read user manual for PN7150, PN7150 needs 3.3v for VBAT power supply.
If i connect 1.8v on hikey board to VBAT(PVDD) of PN7150, what happen? what is phenomenon??
( does it just affect RF performance??)
Should I use the Level Shifter( 1.8v->3.3v) ??
Hi bongsu,
See below, please!
VBAT : MIN --- 2.7V (reader), MAX---5.5V. if you use 1.8V, PN7150 can't normally work.
VDD(PAD): It is PVDD , the voltage is VDDIO , so you can use 1.8V or 3.3V.
PVDD is just IO voltage between HOST, it doesn't afftect RT performance.
Have a nice day!
NXP TIC team Weidong Sun
Thank you for answer.
Unfortunately there is just one common pin(vbat/pvdd) for vbat and pvdd on my pn7150 module board(PN7150BBBM). So i can't seperate pvdd and vbat. To connect hikey board, I think I have to use level shifter(1.8v~3.3v) for pvdd/vbat and i2c , gpios because hikey board doesn't support 3.3v.
is this right solution?