Hi all,
I seem to have a problem to understand restrictions and limits of the INH pin of the TJA1101. Namely, page 37 of the datasheet clearly says that "output current on pin INH" is -2mA. However, on the page 42 there is a small section about INH pin where it is given Voh, Iol and leakage current. What does Iol - LOW-level output current mean exactly. It is given under conditions that Vinh = 0 and can be -15ma -7ma -2ma (min, typ, max).
Hi
Iol means if pull INH down '0' from external mandatory there is maximum 15mA current draw from INH.