AnsweredAssumed Answered

Connecting Bluetooth to S32V234 board

Question asked by NURUL HIDAYAH on Feb 24, 2019
Latest reply on May 22, 2019 by Paul Vlase

Hi..

I'm currently using SBC-S32V234 board for my project. I need to add a bluetooth communication interface to the board, to communicate with my phone..

Is it possible to connect a hc05 bluetooth module to the micro USB port provided on the board?

I can see that the micro USB are connected to also UART interface..

With some micro USB - TTL conversion, can the bluetooth works on the board without changing its firmware/kernel?

 

Thank you in advanced

Outcomes