AnsweredAssumed Answered

LPCXpresso845MAX FreeRTOS

Question asked by Eddie Vazquez on Feb 22, 2019
Latest reply on Jun 29, 2020 by Ed Sewell

Hello community,

 

I am currently using the above board based on LPC845 with Cortex M0+ core, I was wondering if there is an example project of basic FreeRTOS for this microcontroller such as the one in Debug freertos_blinky (also it is mentioned here but never linked so a link to the FreeRTOS example used would be nice) . Or can this one be used for this board?? I am using sdk and MCUxpresso IDE. Precisely I would like to know if there are ports for this micro? If not a slight overview of how difficult and the overall process to port a FreeRTOS for M0+ of another micro would be ?

 

 

Thanks a lot.

 

Eddie

Outcomes