AnsweredAssumed Answered

Can "S32 DS with JLink Jtag" program s32K144?

Question asked by Kevin Lau on Feb 19, 2019
Latest reply on Feb 25, 2019 by stanish

Hi Dear Reader(s),

 

I have written some programs on the S32K144EVB board using  IDE S32 Design Studio -"S32DS_ARM_Win32_v2018.R1_b180326".

 

We have designed our board with a s32K144 on it.  Before I get these boards (later this week), I want to find out if I can program the S32K144 with "S32 DS with JLink Jtag".

 

So I connected the JLink Jtag to the "OpenSDA/JTAG"  on the evaluation board, that killed all green leds. I think that may kill the board power also, then I stopped.

 

Next I connected the JLink Jtag to the SWD connector on the evaluation board, I saw the leds on the JLink Jtag blinked, and S32 Design Studio output messages that look like the processor has been re-programmed, but I did not have control on the debug menu like "step", "run", and "halt".

 

Based on what I saw, it seemed that "S32 DS with JLink Jtag" can NOT program our board with s32k144 on it.

 

Am I correct?  Do I need to get help from IAR or Keil?

 

Thanks,

Kevin

Outcomes