MPL115A2 Coefficients

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPL115A2 Coefficients

Jump to solution
1,360 Views
beng_
Contributor III

I've just started experimenting with the MPL115A2 Digital Barometer.

Maybe I’m having a bad day – but I can’t understand how to convert the Coefficient integers / binary values into numbers.

The data sheet doesn’t seem to make sense. For example a0 is defined as

a0 Signed, Integer Bits = 12, Fractional Bits = 3 : Coeff a0 = S I11 I10 I9 I8 I7 I6 I5 I4 I3 I2 I1 I0 . F2 F1 F0

Later the data sheet uses the example a0 = 0x3ECE = 2009.75

Maskign out - bits I11 to I0 gives 2009 - but the last 3 bits (the fractional bits) are 0x06 - I can't see how that taken to be 0.75?

Are there any examples of how to take these Coefficients in binary/hex form and convert them into actual numbers?

Labels (1)
Tags (2)
1 Solution
1,189 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ben,

As for the fractional part, F2 = 0.5, F1 = 0.25 and F0 = 0.125.

Considering our example, the fractional part is 0b110 = 1 x 0.5 + 1 x 0.25 + 0 x 0.125 = 0.75

You may find useful David's example project, have a look at MPL115A1.c file.

I hope it helps.

Best regards,

Tomas

View solution in original post

4 Replies
1,190 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Ben,

As for the fractional part, F2 = 0.5, F1 = 0.25 and F0 = 0.125.

Considering our example, the fractional part is 0b110 = 1 x 0.5 + 1 x 0.25 + 0 x 0.125 = 0.75

You may find useful David's example project, have a look at MPL115A1.c file.

I hope it helps.

Best regards,

Tomas

1,189 Views
beng_
Contributor III

That works for the first Co-effeicent a0 - but not the next one b1. In the data-sheet:

0xB3F9 = -2.37585

0xB3F9 = 1011 0011 1111 1001

There's one sign bit - 1 - so the number is negative

Two Integer bits - 01 - so the integer portion is 1 (not 2 according to the datasheet)

13 Fraction bits - 1 0011 1111 1001 - (this is 0.5 + 0.0625 + 0.03125 + 0.015625 0.007815 etc...) so the integer portion is 0.62414551 (not 0.37585 according to the datasheet).

0 Kudos
1,189 Views
beng_
Contributor III

Never mind got it - there's a later note in the data sheets that says:

NOTE: Negative coefficients are coded in 2’s complement notation.

Taking the bit inverse of all bits gives me the correct answer

0 Kudos
1,189 Views
beng_
Contributor III

Ah ha - thanks - that makes sense!

0 Kudos