My task is to design a antenna to read a mifare tag.
I try to describe the application:
Imagine a credit card shaped tag, but way smaller (25mm long, 11mm high, 3mm thick). This tag travels trough a tube with 15mm ID. This limits the turn of the card to the Z-Axis. So seen from a 0 degree point, the card can have any particular degree of turn from 0-359 degree.
At the postion of the reader, the card will be stopped, but cannot brought to a defined angle.
The reader antenna must be placed around the tube and has to be able to read the tag in any particular angle of Z.
Which antenna type/shape would be reccomended for this application? Maybe someone here knows about a similar application design.
Any help is appreciated
I'm using the CLRC663
which chip are you using?