AnsweredAssumed Answered

yocto  add pam module

Question asked by 一海 陈 on Feb 18, 2019
Latest reply on Feb 19, 2019 by igorpadykov

hi,

   How can make the  pam module to rootfs?  i use imx6  yocto enviroment!

  1. i  add this in the local.conf

 IMAGE_INSTALL_append += " pam"

  2. then,  bitbake fsl-image-qt5.   and the error :

ERROR: Nothing RPROVIDES 'pam' (but /work/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'pam' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['pam']
ERROR: Required build target 'fsl-image-qt5' has no buildable providers.
Missing or unbuildable dependency chain was: ['fsl-image-qt5', 'pam']

 

i found  pam at path :  poky/meta/recipes-extended/pam. but  i do not known  how to do . is some one 

came the same problem.  

 

thanks a lot!

Outcomes