hi i have developed the card reader device using mfrc630plus,
Our device can read and write mifare classic card.
but desfire, jcob card doesn't response about request ALL.
I not sure that this issue is about h/w (tuning) or f/w (register setting) etc...
h/w developer is said that the antenna tuning is not perfect but well.
I will wait to your advice.
Hello All,
I am also using MFRC630plus reader chip with MSP430 Microcontroller,
As i understand you were able to read the Mifare classic card using the reader chip,
I would request if possible can you please help me as i am stuck up with this,
Please share if any reference or bare minimal code if possible which i can refer and test the basic reading functionality with mifare classic card
Thanks and Regards
Santosh P
We provide sample projects for desfire in the NFC reader library, and you may request from the docstore.
Please refer to the attachment for more details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------