Hi Tom
Thanks for the reply.
No - I am just using File Open menu in Code Warrior and navigating to the .elf file and loading it in. This is what the MC56F8xxx/DSP5685x Targeting Manual tells me, in section Debugging for DSP56800E, section 'Loading an .elf File Without a Project' (pg. 185). When I press the green arrow to start, I get this message. I have changed a number of options so that they look the same as those on a project that builds and downloads OK, but it still doesn't work.
One other question: I have noticed the Code Warrior and command line linkers behave differently with the OBJECT directive in the linker command file. It seems that the command line linker wants .obj, while Code Warrior linker wants .c, like this:
OBJECT (F_EntryPoint, main.obj) # The function _EntryPoint have to be placed at the beginning of the code
# section for proper functionality of the serial bootloader.
and
OBJECT (F_EntryPoint, main.c) # The function _EntryPoint have to be placed at the beginning of the code
# section for proper functionality of the serial bootloader.
So it will build without error only in one or the other. I guess Code Warrior used a different linker?
Thanks