AnsweredAssumed Answered

Any way to reboot i.MX6 via MfgTool2 WITHOUT returning to serial download mode?

Question asked by Erik Schumacher on Feb 14, 2019
Latest reply on Feb 19, 2019 by Erik Schumacher

I am attempting to reboot an i.MX6 based system after deploying new uboot/kernel/rootfs images via MfgTool2.  I am not on location, so I don't have access to the physical unit in order to perform a hardware reset (which is typically how I exit serial download mode when on location).  I am able to enter serial download mode via uboot using bmode usb, just can't return to normal boot mode when MfgTool2 is completed.

 

I have attempted <CMD state="Updater" type="push" body="!3">Done</CMD>.  However, this just reboots back into serial download mode.

 

Is there a different command available that lets me reboot and exit serial download mode?

Outcomes