Kernel 4.14.78, clock-provider and m41t80.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kernel 4.14.78, clock-provider and m41t80.c

722 Views
patrick_schneid
Contributor I

Hi everyone,

we are using an RTC which depends on the m41t80 kernel driver. This RTC has a CLK-OUT feature which is per default to ON and 32kHz. We have another chip wired and depending to that clock signal.

On kernel version 4.1.15 there was no feature to enable/disable square wave output for this rtc driver, so it was always on per default.

On the new linux-imx 4.14.78 kernel, there was a patch:

adding clock-provider feature linux-imx - i.MX Linux kernel 

Which results in the clock output signal being turned of as default option. Now I am totally lost on how to activate that feature in - I think the device tree?

I am not finding proper documentation on that matter. I tried adding clock attributes in the dts but with no luck so far. My entry is:

/* external real time clock */
i2c_rtc: rtc@68 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_rtc_int>;
compatible = "st,rv4162", "fixed-clock", "microcrystal,rv4162";
reg = <0x68>;
interrupt-parent = <&gpio5>;
interrupts = <1 IRQ_TYPE_LEVEL_LOW>;
status = "okay";
#clock-cells = <1>;
clock-frequency = <32678>;
clock-output-names = "rtcosc";
};

Any help appreciated!

Regards,

Patrick

Labels (1)
0 Kudos
1 Reply

525 Views
jimmychan
NXP TechSupport
NXP TechSupport

I would suggest you can replace it by the old one if you don't need the new features of the driver.

If you need the new driver, it is better to ask ST for the document how to set it up in the devicetree.

0 Kudos