We use LPC435X processor and would like to use the USB ROM stack and use NXBUSBlib. We used
www.lpcware.com/content/project.nxpUSBlib to download the source code and couldn’t find there. Where I we find source code for NXBUSBLib and also manual for using USB ROM stack?
Thanks
LlPC435X still support USB ROM Stack for HID or communication class?
Hi
There is USBD Library for LPC4300/LPC1800 series MCUs
https://www.nxp.com/docs/en/application-note/TN00041.zip
Please check if this can help you.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank Jun Zhang.
As we mentioned, we are using LPC4357 and want to use one UBS controller as a host and communicate using Mass Storage class and another one in device mode and use either HID or communication (want to connect to a window host and window host can send configuration info to our board through this port). Do have any vendor suggestions which support dual mode USB driver ? Since we want to use one controller as host and another one as device we are guessing OTG mode won't work for us.
Thanks
Thesycon is a very good provider of USB stacks for the LPC1800 and LP4300:
Regards,
Bernhard.
Hi SS,
I was informed we stopped maintaining lpcusblib and there is no support provided.
If user needs usb demo code, please use lpcopen which can be downloaded from this url
LPCOpen Software for LPC43XX | NXP
Thanks for your understanding.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------