AnsweredAssumed Answered

MIddleware not accessible in New Project for MCUX IDE 10.3

Question asked by Tom Moulton on Feb 12, 2019
Latest reply on Feb 13, 2019 by LPCX presso support

When using the New Project wizard with IDE 10.3 and SDK 2.5 the LWIP and FATFS are not available in the middleware section.

 

Ironically wolfSSL is there, which is kinda hard to use without lwip...

 

Is this a bug or a management decision?

I saw this comment in another thread 

 Unfortunately NXP does not have a plan to add the snmp demo into SDK due to the maintenance reasons.
I would suggest you implement it by yourself, please refer to below link.

Daniel Chen 

 

Thanks

Tom

Outcomes