Hello All,
i am using T2081 custom board based on T2080RDB-PC board.
in RDB Board i have Nor Flash(JS28F00AM29EWHA),which i am able to flash with Codewarrior,
but in my custom board Nor Flash is MT28EW01GABA1LPC,so do i have to make any change while flashing with codewarrior.
i have created build for T2080 RDB board,can i use the same build for T2081 QDS board.
How to create the build for T2081 borad.i am not getting any command to build for T2081QDS in SDK Documentation.
Thanks & Regards,
Anshul Khare
It looks like that Flash programmer setting for the JS28F00AM29EWHA can be used for the MT28EW01GABA1LPC.
See Also FlashToolKit in CodeWarrior 10.5.1 folder.
See the Section 4.4.17 of SDK 2.0-1703 documentation:
https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf
This Section contains information about using SDK 2.0 on the T2080QDS board.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------