AnsweredAssumed Answered

FRDM-KW24D512 un-responsive after Bricking in Windows10

Question asked by sgrmtb@kashmiruniversity.ac.in on Feb 4, 2019
Latest reply on Feb 6, 2019 by Mario Ignacio Castaneda Lopez

Board:

      - FRDM-KW24D512

Problem:

      - Out of my four above types of boards, three became unresponsive due to bricking in Windows 10 or while trying to unbrick the bricked ones.or

Condition:

      - When Powering through the OpenLink USB No LED Glows or blinks

      - No drive appears in the Windows (while keeping the reset button pressed or otherwise)

      - When powering through the KW24 USB Two RED LED's Glow

What did I Try:

      - Followed the steps mentioned in DAPLink bootloader update | Mbed  regarding the problem and possible solutions using External Debug Probe (ULINK Pro).

      - Downloaded the DPLink Source from DAPLink/DEVELOPERS-GUIDE.md at master · ARMmbed/DAPLink · GitHub and compiled the solution as per the given instructions correctly for the k20dx_frdmkw24d_if as the board used OpenSDA MCY named K20DX128Vxx5. 

      - I used the following settings for the Options for the Target:

 

      - The uVision solution compiled correctly without any error, see the Build Window below:

      - I Flashed the Program, It again worked without any error. See the Build Window Below.

 

However, the Board did not come out of the Bricking State. THE SAME Problem Persists.

Outcomes