Hello,
I´m searching for a camera module for our evalboard MCIMX6SX-SDB (see attachment). Connector J13 has a 40 pin interface.
My problem is, that I don´t find a camera on the market that fits to the connector J13.
Is there a module available on the market?
I want to use the parallel interface of the camera interface
A pin description of J13 would also be interesting.
Thanks!
Best regards
Markus
Hello Markus Willbold,
This board is designed so the Omnivision OV5640/5642 5M Pixel Sensor is used.
The cameras part number and distributor can be found on the following thread:
https://community.nxp.com/message/314081?commentID=314081#comment-314081
“The cameras on the boards come from Omnivision (Ordering Number: OV05640-MRFL-AA0T) and can be ordered through distributor Nu Horizons”.
Although availability may vary. I hope this helps!
Regards,