uja1167 vs uja1169

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uja1167 vs uja1169

1,430 Views
christianhdz
Contributor II

I am trying to compare SBC chips UJA1167 and UJA1169. I want to use the UJA1167 SBC. The problem is I cannot find a document or tool that does this comparison. I see there is a driver already developed in the cookbok for s32k144, which is the sbc_uja1169.h . My guess is that these two chips are very similar but it would be very helpful a document or a tool to compare them and know which registers and fields change between them.

Tags (1)
0 Kudos
1 Reply

1,127 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Juan,

I would recommend taking a closer look at the attached AH1306. Section 12.6 describes software flow differences between UJA1164/7/8/9 SBCs.

Please create a standard ticket if you are interested in the UJA1167 example project which demonstrates how to:

- Program the UJA1167 MTP

- Initialize the UJA1167

- Trigger the watchdog

- Change operation modes

- Handle events etc.

Best regards,

Tomas

0 Kudos