I.MX RT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX RT1064

Jump to solution
1,363 Views
candid
Contributor I

Hello

1) Is RT1064 in mass production?
2) What are the available revisions?
3) Is there a measurement of the real performance of the eMMC interface?
4) Is there a measurement of the real performance of the USB interface as device?

5) Where can download sample projects as mass storage (RT1064 EVK)?

Best regards.

Labels (1)
0 Kudos
1 Solution
1,058 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Sergey Petrov 

1) Is RT1064 in mass production?

Yes, RT1064 is already available on our web page: i.MX RT1064 crossover processor| Arm Cortex-M7| NXP | NXP 


2) What are the available revisions?

It is the first revision A0.


3) Is there a measurement of the real performance of the eMMC interface?

No, there isn't available these measurements yet.


4) Is there a measurement of the real performance of the USB interface as device?

No, unfortunately, there isn't available measurements of this.

5) Where can download sample projects as mass storage (RT1064 EVK)?

The RT is supported in the SDK software package: Welcome | MCUXpresso SDK Builder 

Hope this helps

Regards

View solution in original post

1 Reply
1,059 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Sergey Petrov 

1) Is RT1064 in mass production?

Yes, RT1064 is already available on our web page: i.MX RT1064 crossover processor| Arm Cortex-M7| NXP | NXP 


2) What are the available revisions?

It is the first revision A0.


3) Is there a measurement of the real performance of the eMMC interface?

No, there isn't available these measurements yet.


4) Is there a measurement of the real performance of the USB interface as device?

No, unfortunately, there isn't available measurements of this.

5) Where can download sample projects as mass storage (RT1064 EVK)?

The RT is supported in the SDK software package: Welcome | MCUXpresso SDK Builder 

Hope this helps

Regards