AnsweredAssumed Answered

Build Minimal u-boot binary for t4160rdb board

Question asked by vinothkumar s on Feb 2, 2019
Latest reply on Feb 8, 2019 by vinothkumar s

Hi All,

 

I am using t4160rdb board with Lauterbach. Now this board have ddr controller issue. So, I want to flash into sram. because of this, I built the minimal image ( secondary program loader (spl))

 

Now, I have the doubt, 

 

I built this binary by setting T4240RDB_SDCARD_defconfig in machine configuration file. And I check u-boot  code CONFIG_SDCARD macro also set. 

 

Is it possible to flash u-boot-spl.bin (160 KB) through the NOR flash into SRAM ?

 

If it not, why ? or if it yes, how?

 

If it possible, please provide steps to build minimal u-boot for NOR flash

 

 

Regards,

VinothS

Outcomes