Hi,
I got this nxp gpu sdk from here.
I downloaded it and build 01_SimpleTriangle by Makefile.x11.
Then I executed it on our imx6dl board, I found that it use up to 80% CPU resource.
However, I found it can executed by GPU because CPU usage decrease to 4~10% after I test some method on board
But I cannot confirm how to do it and I cannot repeat this situation when I create new terminal on board.
How to executed this sample by GPU?
Thanks!
Hi Jerry
one can check that gpu driver is included in image, it is described
in linux documentation (Linux Manual) on below links
Linux L4.14.78_1.0.0 Documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------