AnsweredAssumed Answered

Build AGL demo platform Failed for imx8

Question asked by Tung Nguyen Thanh Employee on Jan 30, 2019
Latest reply on Jul 29, 2019 by Manivannan s

Hi expert,

 

I am building AGL demo platform for imx8 following this guide: meta-nxp-agl - i.MX Yocto Project AGL Demo Layer , 

but I got some error while building. The log build as below:

 

ERROR: agl-service-data-persistence-1.0+gitAUTOINC+7147b65d07-r0 do_configure: Function failed: do_configure (log file is located at /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/temp/log.do_configure.15534)
ERROR: Logfile of failure stored in: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/temp/log.do_configure.15534
Log data follows:
| DEBUG: Executing shell function do_configure
| -- The C compiler identification is GNU 7.3.0
| -- The CXX compiler identification is GNU 7.3.0
| -- Check for working C compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-gcc
| -- Check for working C compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-gcc -- works
| -- Detecting C compiler ABI info
| -- Detecting C compiler ABI info - done
| -- Detecting C compile features
| -- Detecting C compile features - done
| -- Check for working CXX compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-g++
| -- Check for working CXX compiler: /data/workspace/linux-auto/imx8qxp-build/tmp/work/aarch64-poky-linux/agl-service-data-persistence/1.0+gitAUTOINC+7147b65d07-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux/aarch64-poky-linux-g++ -- works
| -- Detecting CXX compiler ABI info
| -- Detecting CXX compiler ABI info - done
| -- Detecting CXX compile features
| -- Detecting CXX compile features - done
| CMake Error at conf.d/cmake/config.cmake:204 (include):
| include could not find load file:
|
| CMakeAfbTemplates
| Call Stack (most recent call first):
| CMakeLists.txt:21 (include)

 

Even built for imx6qpsabreauto, I still got the same error.

Can anyone help me to fix it?

 

Many thanks!

Tung.

Outcomes