imx8: alsamixer and no controls

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8: alsamixer and no controls

2,220 Views
reyhanehyazdani
Contributor II

I'm currently running Freescale BSP on imx8mqevk(4.9.88-imx_4.9.88_2.0.0). 

Now, I have a problem with audio controlling. The speaker itself is working fine but there's no volume control. I could play audio files via aplay command but opening up alsamixer just says "This sound device does not have any controls".

here is the list of the detected sound cards:

$ cat /proc/asound/cards

0 [wm8524audio ]: wm8524-audio - wm8524-audio
                              wm8524-audio
1 [imxspdif ]: imx-spdif - imx-spdif
                     imx-spdif
2 [imxhdmiarc ]: imx-hdmi-arc - imx-hdmi-arc
                           imx-hdmi-arc
3 [imxaudiohdmi ]: imx-audio-hdmi - imx-audio-hdmi
                              imx-audio-hdmi

Any assistance would be appreciated.

Reyhaneh

1 Reply

1,459 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, this could be due to the Audion codec that the i.MX8MQ-EVK has is too simple. The driver could not has the functionality to modify the Audio configuration of the codec. What you could make is modify the asound.conf file to modify the default sound configuration. However, I am not quite sure if this could also work. I apologize for the inconveniences this could give you.

Best Regards,

Diego.