AnsweredAssumed Answered

HOW TO simplification NHS3100 Tlogger project

Question asked by 向 雪姣 on Jan 27, 2019
Latest reply on Feb 1, 2019 by matt li

I download the latest version of nhs3100 SDK, and download the tlogger project to my demo board with nothing changed .

 

Memory region Used Size Region Size %age Used
Flash30: 15564 B 30 KB 50.66%
SRAM8: 2980 B 8176 B 36.45%

 

After download the program ,there are only  15156 bytes left for data storage .with these memory ,there are only 82464 temperature data can store .

If I set the meameasurement interval 1 second , with these left storage ,3100 just can work one day .

so ,I want to know ,is there any methods to simplify the tlogger project ?

I need more memory left after download the program .

who can help me ?

tks

 

Outcomes