IMX6QP视频播放

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6QP视频播放

1,511 Views
kentsun
Contributor II
下面是用 nxp的开发板MX6QP-SDB测试的方法和结果:
硬件平台:
MX6QP-SDB
SDK版本:
Linux  4.9.88-imx_4.9.88_2.0.0 
测试流程:
SDK已repo sync到最新版本,
编译采用如下配置:
MACHINE=imx6qpsabresd DISTRO=fsl-imx-fb source ./fsl-setup-release.sh -b eglfs-imx6qp
bitbake fsl-image-qt5-validation-imx
只为增加qtmultidia进行了一些配置修改,与内核相关的任何内容都未有改动。
编译得到包含Qt5Multimedia的镜像文件fsl-image-qt5-validation-imx-imx6qpsabresd.sdcard,写入SD卡中,启动MX6QP-SDB
修改uboot参数video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32
运行一个最简单采用qml播放视频的程序,分别播放2个文件,视频切换时立即出发内核警告如下:
1.jpg
与我们目前用的4.1.15版本SDK类似。
下面是我们自己的板子在进行相同测试时的内核警告信息:
2.jpg
该现象只会出现在IMX6QP上,同样配置的IMX6DL和IMX6Q都不会有问题,请协助分析解决。
为测试方便,我只播放了很短(10秒)的视频文件,附件分别是我们用来测试的qml程序源码和内核日志文件。
0 Kudos
1 Reply

1,178 Views
igorpadykov
NXP Employee
NXP Employee

Hi kent

one can try patch below

[meta-freescale] [PATCH 2/4] gstreamer1.0-plugins-bad: Add i.mx specific code about qmlglplugin 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos