Hi,
The reset value after boot of the SRAM1 bit in AHBCLKTRL0 in LPC546xx according to UM10912 is 0. This means the clock to the SRAM1 is disabled after reset. I however need this clock signal to be enabled in the startup sequence. How can I enable this bit using assembler code in the startup file? Are there examples out there that already do this that I can just copy?
Many thanks
Dani
Hi,
This bit is set after reset.
I have tested the LPC54608 board with our SDK code, after reset, the AHBCLKCTRL0 is really 0X18B,
I also attach my debug test result, you can find both IAR and MDK project, after reset, the AHBCLKCTRL0 is 0X18B,
I reported this issue.
Regards
Sol
Hi Sol
I do not have access to the provided links.
Dani
Hi Sol
Got it now. Thanks
Dani