AnsweredAssumed Answered

Gcc make missing on LS1021ATSN-PA OpenIL image

Question asked by raphael grandpierre on Jan 24, 2019
Latest reply on Mar 31, 2019 by Yiping Wang

Greetings

 

I use a LS1021ATSN-PA with the provided OpenIL 1.3.1 from NxP website.

 

I need to develop application on it, and in particular I need to develop  Xenomai applications  which is provided.

 

The problem is that this image doesn't include a compiler toolchain (gcc, make...) neither a package installer tool.

 

I have installed a linaro cross compilation tool chain, but unfortunately it is complex to cross compile xenomai, so I am asking if someone can tell me how the OpenIL image has been build or how to install gcc (and all the lib) on the LS1021A ATSN-PA.

 

I have read carefully the OpenIL 1.3.1 (OPEN-LINUX-IND-UM-1-3-1.pdf) but it doesn't give information about the compilation chain : this document implicitly suppose a native OpenIL compilation since it says to do "git clone" and then "make"....

 

Thank you very much for your help,

Best regards,

Raphael

Outcomes