Hi All,
We are debugging u-boot using trace32 on our new processor board with an T4240RDB.
We are currently blocked in our development. We are having problems with Trace32 debugger
hardware breakpoints
Here the situation:
We understand that in order to get hardware breakpoints to work we need:
1- A valid address with a valid instruction at IPVR
2- DE bit enable in MSR register
3- To avoid problems; always set breakpoints before or after code which accesses SRR0 and SRR1, and never step through such code.
We have also verify that:
u-boot,
lis r6,MSR_IS|MSR_IS|MSR_DS|MSR_IS|MSR_DE@h
ori r6,r6,MSR_IS|MSR_IS|MSR_DS|MSR_IS|MSR_DE@l
lis r7,switch_as@h
ori r7,r7,switch_as@l
mtspr SPRN_SRR0,r7
mtspr SPRN_SRR1,r6
rfi
After rfi instruction, jump to 0xEFFFF574 but, there is no data present and also all address same like that (data :??????????????)
Thank you,
VinothS
Solved! Go to Solution.
Hi Reinhard,
Thank for your reply and Instruction execute when change MSR to 0.
Regards, VinothS
Hi VinothS,
it seems some of the prerequisites you mention are for e500 cores and do not apply to e500mc/e5500/e6500 cores.
Please contact your local TRACE32 FAE for assistance. You can find the contact information here:
TRACE32® Worldwide Representation
Best regards,
Reinhard
Hi Reinhard,
Thank for your reply and Instruction execute when change MSR to 0.
Regards, VinothS
Hi,
Finally this one fixed by minimal u-boot binary (u-boot-spl.bin) instead of normal u-boot for sram.