AnsweredAssumed Answered

IMX6Q Android6.0 Camera can't capture hight resolution picture well

Question asked by leavs lee on Jan 23, 2019
Latest reply on Feb 21, 2019 by Diego Adrian Cuevas

Hi team,

I am using imx6q based hardware with Ov5640 module is connected to IPU1 CSI0 8bit [CSI0_DAT12  --- CSI0_DAT19] parallel camera interface.  Now, I can get Ov5640 to capture less then 1024x768 resolution pictures, but the resolution which is 1280x720 or higher don't work well. like follow picture.

 

I test follow resolution:

640x480  -- OK

1024x768 -- OK

1280*720 --  don't work well

1920x1080  -- don't work well

2592x1944 -- don't work well

 

I got follow kernel message:

Warnning:

=======

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001

 

Can you help me solve this problem??

Outcomes