Hello,
I can enable the Pin for digital filter in the pin_mux Component.
But is it possible to configure the port digital filter clock and the port digital filter witdth with the Processor expert in the S32Ds for S32K144?
Br Lutz
Hello,
It can't be done in Processor Expert, however, there is a function for that.
void PINS_DRV_ConfigDigitalFilter(PORT_Type * const base, const port_digital_filter_config_t * const config);
For more information please refer to the SDK documentation in the S32DS installation folder.
...\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_BETA_2.9.2\doc\Start_here.html
Regards,
Daniel