你好,MMZ25332B和MMZ2733BT1这两款放大器可以工作在1300mhz吗

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

你好,MMZ25332B和MMZ2733BT1这两款放大器可以工作在1300mhz吗

474 Views
hxt028
Contributor I

参数表写的是1500-2800mhz,用在1300mhz放大可行吗?

Labels (1)
  • RF

Tags (1)
0 Kudos
1 Reply

374 Views
LPP
NXP Employee
NXP Employee

The datasheet provides performance data measured in NXP test circuit. We have no a design for different frequencies and thus we can not provide measured performance data at 1300MHz.

The device product page provides S-parameters that you can use for designing your board.

MMZ25332B|1500-2800 MHz, 26.5 dB Amplifier | NXP 

Have a great day,
Pavel

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos