hi everyone i have MCIMX6SX-SDB (Machine model: Freescale i.MX6 SoloX SDB RevB ) type board with Linux version 4.1.15 (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.9) I try use wi-fi module Intel 4965AG and Ericsson H039R but no success.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hi everyone i have MCIMX6SX-SDB (Machine model: Freescale i.MX6 SoloX SDB RevB ) type board with Linux version 4.1.15 (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.9) I try use wi-fi module Intel 4965AG and Ericsson H039R but no success.

542 Views
o_scherbinin
Contributor III

i have MCIMX6SX-SDB (Machine model: Freescale i.MX6 SoloX SDB RevB ) type board with Linux version 4.1.15 (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.9)
I try use wi-fi modules Intel 4965AG and Ericsson H039R but no success.
In my starting kernel log i have:
imx6q-pcie 8ffc000.pcie: phy link never came up
imx6q-pcie 8ffc000.pcie: failed to initialize host
imx6q-pcie: probe of 8ffc000.pcie failed with error -22
lspci command returns nothing.
I do not see "pcie treaning sets" ( interrogation on PCIE_TX_N & PCIE_TX_P pins, i try it by osciloscope with 600MHz bandwidth)


in my config file i have options:
#Bus support
#
CONFIG_PCI=y
# CONFIG_PCI_DOMAINS_GENERIC is not set
CONFIG_PCI_SYSCALL=y
CONFIG_PCI_MSI=y
# CONFIG_PCI_DEBUG is not set
# CONFIG_PCI_REALLOC_ENABLE_AUTO is not set
# CONFIG_PCI_STUB is not set
# CONFIG_PCI_IOV is not set
# CONFIG_PCI_PRI is not set
# CONFIG_PCI_PASID is not set

#PCI host controller drivers
#
CONFIG_PCIE_DW=y
CONFIG_PCI_IMX6=y
# CONFIG_PCI_IMX6_COMPLIANCE_TEST is not set
# CONFIG_EP_MODE_IN_EP_RC_SYS is not set
CONFIG_RC_MODE_IN_EP_RC_SYS=y
# CONFIG_PCI_IMX_EP_DRV is not set
# CONFIG_PCI_HOST_GENERIC is not set
# CONFIG_PCI_LAYERSCAPE is not set
# CONFIG_PCIE_IPROC is not set
CONFIG_PCIEPORTBUS=y
# CONFIG_PCIEAER is not set
# CONFIG_PCIEASPM is not set
CONFIG_PCIE_PME=y
# CONFIG_PCCARD is not set

# MII PHY device drivers
#
# CONFIG_IWLWIFI is not set
CONFIG_IWLEGACY=y
CONFIG_IWL4965=y

# Bluetooth device drivers
#
CONFIG_MAC80211=y

Thank you,
Oleg.

0 Kudos
2 Replies

428 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Oleg,

Why are you receiving this:

"

imx6q-pcie 8ffc000.pcie: phy link never came up

"

if like configuring like i.MX6Q you have the iMX6SX. Or maybe I´m missing something.

The MX6SX does not have PCI.

Regards

0 Kudos

428 Views
o_scherbinin
Contributor III

hi Bio_TICFSL.

I can't  explain why log has "imx6q-pcie" but can see this for other MX6SX boards here.
For example, https://community.nxp.com/message/858168#comment-858450
So i assume it is correct.
Recently noticed the absence of supply VGEN2_1V5 (mpcie_1v5). This provide MMPF0200F6AEP and seems it is not enable by default.

0 Kudos