I am using ENET2_TX_CLK as USB OTG2_ID now.
What is the value of MX6UL_PAD_ENET2_TX_CLK__ANATOP_OTG2_ID in device tree system?
pinctrl_usbotg2: usbotg2grp {
fsl,pins = < MX6UL_PAD_ENET2_TX_CLK__ANATOP_OTG2_ID ?value?
>;
};
Hi liangfeng_0824
one can set it to the same value as for *ANATOP_OTG1_ID in example on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
What is the difference between imx6ul-14*14-evk board hardware and imx6ul-14*14-ddr3-arm2 hardward ?
imx6ul-14*14-ddr3-arm2 is internal validation board, imx6ul-14*14-evk board
was developed for customers use.
Best regards
igor
i use imx6ul platform ; Can you reply me as soon as possible?