MSCAN Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSCAN Question

480 Views
edison_wu76
Contributor I

Hi Sir,

IC:mc9s12xet256 

Output:CAN4 = PIN117(TXD),PIN118(RXD)

I try to use the MSCAN Rx interrupter, IC always not pass at "EnableInterrupts;".

please help me , what happen ?

thanks so much.

#include <hidef.h> /* common defines and macros */
#include "derivative.h" /* derivative-specific definitions */
#define ST_ID_100 0x100

#define ACC_CODE_ID100 0x2000
#define ACC_CODE_ID100_HIGH ((ACC_CODE_ID100 & 0xFF00)>>8)
#define ACC_CODE_ID100_LOW (ACC_CODE_ID100 & 0x00FF)

/* Mask Code Definitions */
#define MASK_CODE_ST_ID 0x0007
#define MASK_CODE_ST_ID_HIGH ((MASK_CODE_ST_ID & 0xFF00)>>8)
#define MASK_CODE_ST_ID_LOW (MASK_CODE_ST_ID & 0xFF)
/* Task FlagDefinitions */
unsigned char Task_CAN =0x00;
unsigned char errorflag;
unsigned char txbuff[8] ="12345";
unsigned char rxbuff[8] ="";
unsigned int rxID;
/* Function Definitions */
void Task(void);

/* MSCAN0 Init */
void can4Init()
{
//MSCAN Initial mode
CAN4CTL0 = 0x01;

//Check Entry the MSCAN Initial mode
while(!(CAN4CTL1 & 0x01));

//MSCAN Enable & Loop Enable
CAN4CTL1 = 0x80;

//fOSC=4MHz,CAN speed=250kbps
CAN4BTR0 = 0xC0;
CAN4BTR1 = 0x67;

/* Close Filters */
CAN4IDAC = 0x30;
CAN4IDAR0=CAN4IDAR1=CAN4IDAR2=CAN4IDAR3=0xFF;
CAN4IDAR4=CAN4IDAR5=CAN4IDAR6=CAN4IDAR7=0xFF;
CAN4IDMR0=CAN4IDMR1=CAN4IDMR2=CAN4IDMR3=0xFF;
CAN4IDMR4=CAN4IDMR5=CAN4IDMR6=CAN4IDMR7=0xFF;
//CAN0IDAR0 = ACC_CODE_ID100_HIGH; //|\ 16-bit Filter 0
//CAN0IDMR0 = MASK_CODE_ST_ID_HIGH; //| \__ Accepts Standard Data Frame Msg
//CAN0IDAR1 = ACC_CODE_ID100_LOW; //| / with ID 0x100
//CAN0IDMR1 = MASK_CODE_ST_ID_LOW; //|/
/* Acceptance Filters */
//CAN0IDAC = 0x10; /* Set four 16-bit Filters */
//CAN0IDAR2 = 0x00; //|\ 16-bit Filter 1
//CAN0IDMR2 = MASK_CODE_ST_ID_HIGH; //| \__ Accepts Standard Data Frame Msg
//CAN0IDAR3 = 0x00; //| / with ID 0x100
//CAN0IDMR3 = MASK_CODE_ST_ID_LOW; //|/
//CAN0IDAR4 = 0x00; //|\ 16-bit Filter 2
//CAN0IDMR4 = MASK_CODE_ST_ID_HIGH; //| \__ Accepts Standard Data Frame Msg
//CAN0IDAR5 = 0x00; //| / with ID 0x100
//CAN0IDMR5 = MASK_CODE_ST_ID_LOW; //|/
//CAN0IDAR6 = 0x00; //|\ 16-bit Filter 3
//CAN0IDMR6 = MASK_CODE_ST_ID_HIGH; //| \__ Accepts Standard Data Frame Msg
//CAN0IDAR7 = 0x00; //| / with ID 0x100
//CAN0IDMR7 = MASK_CODE_ST_ID_LOW; //|/

/* Exit Initialization Mode Request */
CAN4CTL0 = 0x00;

/* Wait for Normal Mode */
while ((CAN4CTL1&0x00) != 0);
}
unsigned char can4ReadFrame(void)
{
unsigned char length, index;
// unsigned char rxdata[8];
// unsigned int rxID;
unsigned char rxRTR;
unsigned char IDE;

if(CAN4RFLG & CAN4RFLG_RXF_MASK) return(0);
// if no new message=>return
//if(!(CAN4RFLG & CAN4RFLG_RXF_MASK)) return(0);
// if not standard identifier=>return
//if(CAN4RXIDR1 & 0x08) return(0);
// if not data frame=>return
//if(CAN4RXIDR1 & 0x10) return(0);

/* Get Can ID */
rxID= CAN4RXIDR0;
rxID= (rxID<<3) + (CAN4RXIDR1>>5);
/* Get received data */
length = (CAN4RXDLR & 0x0F);
for (index=0; index<length; index++)
rxbuff[index] = *(&CAN4RXDSR0 + index);

CAN4RFLG = CAN4RFLG_RXF_MASK;

return 1;
}
unsigned char can4SendFrame(unsigned long id, unsigned char priority, unsigned char length, unsigned char *txdata)
{
unsigned char txbuffer;
unsigned char index;

//Check TXE Buffer
if(!CAN4TFLG) return 1;

//Set TXE Buffer
CAN4TBSEL = CAN4TFLG;
txbuffer = CAN4TBSEL;

//Write ID
*((unsigned long *) ((unsigned long)(&CAN4TXIDR0))) = id;
CAN4TXIDR0=0B10101010;
CAN4TXIDR1=0B10100111;


//Write Data
for (index=0;index<length;index++) {
*(&CAN4TXDSR0 + index) = txdata[index];
}
/* Set Data Length Code */
CAN4TXDLR = length;
/* Set Priority */
CAN4TXTBPR = priority;

/* Start transmission */
CAN4TFLG = txbuffer;

/* Wait transmission */
while ( (CAN4TFLG & txbuffer) != txbuffer);
}
void Delay (void) {
unsigned int counter;
for (counter=0;counter<50000;counter++);
}
#pragma CODE_SEG NON_BANKED

void interrupt VectorNumber_Vcan4rx IQR_INT(void) {
unsigned char length, index;
unsigned char rxdata[8];

length = (CAN4RXDLR & 0x0F);
for (index=0; index<length; index++)
rxdata[index] = *(&CAN4RXDSR0 + index); /* Get received data */

CAN4RFLG = 0x01; /* Clear RXF */
}

#pragma CODE_SEG DEFAULT

void main(void)
{

// SET Port-M For CAN4
DDRM_DDRM7=1;
DDRM_DDRM6=1;
MODRR_MODRR2=0;
MODRR_MODRR3=1;
//MSCAN Setting Function
can4Init();
//Wait CAN BUS SYNCH
while (!(CAN4CTL0 & 0x10));
//Clear CAN0 RXF flag
CAN4RFLG = 0x01;
//Enable CAN0 RX interrupt
CAN4RIER = 0x01;
//Enable all interrupt
EnableInterrupts;

for (;;)
{
/* CAN0 Send Data */
// errorflag = can4SendFrame((ST_ID_100), 0x00, sizeof(txbuff)-1, txbuff);
Delay();
//Delay();
// errorflag = can4ReadFrame();
//Task_CAN = can4ReadFrame();
// Task();
}
}
void Task(void)
{
if(Task_CAN & 0x01){
/* CAN0 Send Data */
Task_CAN=can4SendFrame((ST_ID_100), 0x00, sizeof(txbuff)-1, txbuff);
//Delay();
Delay();
Task_CAN=0x00;
}

}

Labels (1)
0 Kudos
1 Reply

321 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Have you tried debugging the code?  

What did you see in "MSCAN Receiver Flag Register (CANRFLG)"?

IC always not pass at "EnableInterrupts;".

What does it mean? Is the MCU resetting or is it in a loop?

Also, the CAN examples for S12XEP100 can be useful: LAMA's S12XE unofficial examples 

Thank you. I hope it helps you.

Best Regards,

Diana

0 Kudos