AnsweredAssumed Answered

K61_256BGA_120MHz_150MHz.bsdl BSDL file for the 32 bit Kinetis K61 (MK61FN1MOVMJ12).

Question asked by Terry Walton on Jan 11, 2019
Latest reply on Jan 16, 2019 by Fang Li

I'm using the K61_256BGA_120MHz_150MHz.bsdl BSDL file for the 32 bit Kinetis K61 (P/N MK61FN1MOVMJ12).. There is no Boundary Scan cell to drive DDR_CK_  on pin A10.  There is a Boundary Scan cell on DDR_CK on pin A11.  Is there actually a cell on pin A10 and the BSDL file is wrong or is there no cell on A10?   A10, DDR_CKB, is defined as a linkage bit.. This is currently preventing me from developing a DDR memory test on the Boundary Scan test project I'm working on. 

Outcomes