AnsweredAssumed Answered

Reset max voltage when there is no supply

Question asked by Nicolas Boucquey on Jan 10, 2019
Latest reply on Jan 17, 2019 by Nicolas Boucquey

Hi,

 

We are trying to figure out if we can apply 5 V on the reset pin of the LPC1837JET100 even if its supply voltage is 0 V.

For other 5 V tolerant pins, the datasheet details that the max voltage is 3.6 V when there is no supply. Is it the same for the reset pin?

 

Many thanks in advance,

 

Nicolas Boucquey

Outcomes