Hi,
I have a question about voltage of VDDARM_IN and VDDSOC_IN during Reset.
VDDARM_IN and VDDSOC_IN are connected together and voltage applied at 1.42V, However, when VDDARM_CAP and VDDSOC_CAP turn on, 1.42V drop to 1.17 in short time during reset.
I think it is no problem because it is during reset and voltage is more than sleep mode voltage 0.9V.
Can you think of something to be a problem?
Best Regards,
Sugiyama
Hi, Yuri,
Thanks for your comment.
Best Regards,
Sugiyama
Hello,
The i.MX6 VDDARM_IN and VDDSOC_IN voltages should not violate corresponding specs in
Operating Ranges tables of i.MX6 Datasheet(s). Also, let me remind, according to Table 2-6 (Power
and decouple recommendations) of Hardware Development Guide for i.MX6:
VDD_SOC_IN requires a 66 uF bulk capacitance.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
HI, Yuri,
Thank you for answer.
Customer already use 66uF for VDD_SOC_IN.
I think voltage of these power line during reset could corresponding to Stand by voltage.
Do you agree this?
Best Regards,
Sugiyama
Generally - yes.