AnsweredAssumed Answered

Can I run multiple pn-7150 on the same (or different) i2c buses with the pn-52xx kernel driver (or HAL)

Question asked by Ryan Sturmer on Jan 9, 2019
Latest reply on Jan 28, 2019 by Jonathan Iglesias

I am integrating the 7150 into my application, and there is need for multiple readers.  I am rifling through the libnfc-nci stack with the intent on using the pn-52xx kernel driver in our application.  It looks to me as if there is no way to support multiple devices on the same system - is this correct?  I would like to have two readers, either on the same i2c bus at different addresses, or possibly on two different busses if this is not possible.  Can this be achieved without substantial modification to the driver, the libnfc layer, or both?

Outcomes