Hi,
After removing external crystal oscillator and using internal RC oscillator of 12MHz PLLed to 72MHz is giving error in printf().
printf() is not giving any output on putty, while TXDATA is working fine.
also the following issue is showing up while stopping or pausing the debug.
No source available for "__vfprintf() at 0x3114"
No source available for "printf() at 0x300a"
port and baud rates have been doublechecked.
IDE : MCUXpressoIDE
Library : REDLIB
Clock : Internal RC Clock PLLed to 72MHz
Processor : LPC1517
Hi ATHMESH NANDAKUMAR,
If you don't use the printf, whether your UART can output the correct data?
I use the official lpc1549 uart_rb project can output the correct uart data:
I just add the printf("TEST");
I also attach my modified project for your reference.
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------