Is there a cfimager that can run on Linux or Mac?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a cfimager that can run on Linux or Mac?

457 Views
paulchen1
Contributor I

Is there a cfimager that can run on Linux or Mac? Same as other .exe tools on Windows.

Thanks for comments

Labels (1)
0 Kudos
1 Reply

389 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

I am afraid such version is not available, may be helpful to use sources

GitHub - NXPmicro/cfimager: Write Freescale/NXP imx sb file or raw data to SD card 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos