We are looking to add some components to the reference design of the i.MX6UL/NXP Modular Gateway for a project and have some clarification questions:
Have there been any revisions or update to the NXP reference design since Schematic Revision 2.05?
Which ports are open/available for use?
Is everything going to being connected through the SO-DIMM Connector Interface(Base Board Schematic pg.7)?
What is the maximum current draw in amps for the 5V input power supply interface (Base Board Schematic pg.3)?
What is the maximum current draw in amps for the 3.3V SW regulator Interface (Base Board Schematic pg.3)?
Thanks!
Hello Aquiel Godeau ,
i.MX6UL/NXP Modular Gateway is designed by 3rd party, See here, please!
https://www.nxp.com/webapp/connect/displayPartnerProfile.sp?partnerId=8660
So please contact them!
Have a nice day!
BR,
weidong