I have setup a bluetooth module to capture data from the LPC through an Arduino. I see a lot of data getting lost, could someone tell me if there is a bluetooth library for nxp's lpc4370?
I have setup a bluetooth module to capture data from the LPC through an Arduino. I see a lot of data getting lost, could someone tell me if there is a bluetooth library for nxp's lpc4370?
Hi Zhang Jennie,
There is no Bluetooth module in the LPC4370, but I am sure I can integrate the MC with a HC05, is UART the only solution?
Thanks!
Hi Visweshwar Srinivasan,
What do you mean "integrate the MC with a HC05, is UART the only solution? " ?
Can you please be more specific?
Jennie Zhang
So I need to transfer data from my nxp microcontroller using UART communication. Could you tell me if that's possible? I have been trying to communicate and have not been able to do so this far, is there an example I could refer?
something like this:
Bluetooth with the Freedom Board | MCU on Eclipse
or:
Using the HC-06 Bluetooth Module | MCU on Eclipse
?
Hi Visweshwar Srinivasan,
I contacted wireless team, there is no bluetooth library for lpc4370.
NXP has bluetooth solution for these wireless chips:
Bluetooth®Smart/Bluetooth Low Energy|NXP
Have a great day,
Jun Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------