Hello, Nxp community,
I have tried both LSDK 18.09 and 18.12 on ls1012afrwy board. I could boot the Ubuntu and log in by either UART or SSH.
However, I couldn't edit the configure file with VI editor. Whenever I opened a file with VI, VI couldn't show the existing text, and moving the cursor (arrow keys) will end up printing wired character "@k" on the screen instead of scrolling.
Does anyone have the same issue?
Thanks
Hello Zhenchuan Chai,
I can reproduce your problem with Ubuntu 18.04.1 LTS rootfs built from LSDK 1812 release.
Please use vi command provided in busybox, it works normally, please use "busybox vi <your file>".
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Yiping,
Great, it works well.
Thanks for help
Zhenchuan