AnsweredAssumed Answered

Can the Demo Board OM6270 generate UART baud rate of 1Mbit

Question asked by Paul Conroy on Jan 7, 2019
Latest reply on Jan 8, 2019 by G.w. Sun

Hi 

I have an application where I need to initially configure a device over serial uart at 115200 baud and then switch up to 1Mbit baud for the rest of the communication. 

I think a 32Meg xtal will give a good baud rate of 1Mbit, and at 115200 an error of 2.12%, if my calculations are correct.

 

Will the SC16is760 or 750 run at the 1Mbit baud rate successfully over a very short distance?

The device I am communicating with is 5v, will I need series resistor on the receive line?

 

is there a better xtal frequency for both baud rates?

Outcomes