Question about DCD version field on RT106x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about DCD version field on RT106x

690 Views
carstengroen
Senior Contributor II

In the UM for RT1060 it is shown that the Version field of the DCD data must be 0x41:

pastedImage_1.png

However, in the evkmimxrt1060_sdram_ini_dcd.h it is set to 0x40.

pastedImage_2.png

Which one is correct ?

Labels (1)
0 Kudos
2 Replies

562 Views
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

it can be both as described in Figure 8-15

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

562 Views
carstengroen
Senior Contributor II

Thanks Igor,

but that is for the IVT, the one I referenced above is the DCD ?

0 Kudos