LS1043A RCW clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A RCW clarification

930 Views
mike_palmer
Contributor II

Looking at the LS1043A Reference Manual (rev 4, 6/2018), RCW source-encodings (Table 4-9), the QSPI (0_0100_010x) and SD/MMC (0_0100_0000) cfg_rcw_src values are footnoted with "Not valid as an RCW[IFC_MODE] encoding."

Can someone clarify what it meant by this footnote?

Tags (3)
0 Kudos
1 Reply

754 Views
ufedor
NXP Employee
NXP Employee

The mentioned note means that IFC is implicitly initialized in accordance with the RCW source-encoding (the RCW[IFC_MODE] is not used) in all cases except QSPI and SD/MMC when IFC is initialized by the RCW[IFC_MODE].

0 Kudos