AnsweredAssumed Answered

IMX7D PCIE Control Register Access Failure

Question asked by Chris Tsang on Jan 2, 2019
Latest reply on Jan 3, 2019 by Chris Tsang

Hi all,

 

I am working on PCIE support on my custom board. I raised a question before IMX7D PCIE Support . But this time I am going to provide more details.

 

As I am going to enable PCIE support for IMX7D, I have enabled following kernel options.

CONFIG_PCI=y
CONFIG_PCI_MSI=y
CONFIG_PCI_IMX6=y

CONFIG_BLK_DEV_NVME=y

After that I have also enable the PCIE in device tree.

&pcie {
     pinctrl-names = "default";
     pinctrl-0 = <&pinctrl_pcie>;
     reset-gpio = <&gpio1 13 GPIO_ACTIVE_LOW>;
     disable-gpio = <&gpio1 12 GPIO_ACTIVE_LOW>;
     status = "okay";
};

 

After that, the kernel stuck at

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

 

I finally trace the cause is here in pcie-designware.c

void dw_pcie_setup_rc(struct pcie_port *pp)
{
return;
u32 val;
/* set the number of lanes */
val = dw_pcie_readl_rc(pp, PCIE_PORT_LINK_CONTROL);
val &= ~PORT_LINK_MODE_MASK;
switch (pp->lanes) {
case 1:
val |= PORT_LINK_MODE_1_LANES;
break;

The dw_pcie_readl_rc() function cannot proceed and the kernel fails to respond.

 

This issue only happens on my custom board but not on IMX7D sabre board.

 

I tried to manually read the register instead, in both kernel and uboot. Both of them fail to respond and keep stuck at that moment. Even CTRL-C cannot escape that condition

Kernel:

memtool md -l 0x33800710 1

Uboot

md.l 0x33800710 1

 

This register seems to be able to access using certain method. 

 

Please advise. Thanks.

 

Chris Tsang

Outcomes